This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5707 无声音输出

Other Parts Discussed in Thread: TAS5707, TAS5707EVM

我们项目现在用第一次用TAS5707,但调试了几天还是没有声音输出。

电路跟TAS5707EVM 基本一样,电源电压3.3V 和 17V , LRCK  44.3KHZ, SCK  64*44.3KHZ  24BIT 模式 64FS   ,MCLK 12MHZ

I2S的信号量了基本没问题,I2C 对寄存的设置:

X1B 00
X06 00
X04 05
X11 4C
X12 34
X13 1C
X14 64
X20 00 89 77 72
X25 01 02 13 45

X3A 00 7F FF 03 00 00 00 FB
X3B 00 7F FF 03 00 00 00 FB
X3C 00 7F FF 03 00 00 00 FB
X40 FC 83 10 D4
X41 0F C0 00 00
X42 00 08 42 10
X46 00 00 00 00
X08 10
X09 10
X07 47
X53 00 80 00 00 00 00 00 00
X54 00 80 00 00 00 00 00 00
X1A 0A
X07 FF
X05 00

应该也是对的, 播放的 声音文件是一个1K 的声音,但就是没有声音输出,PWM 输出 波形频率是300KHZ.DATASHEET上说是 384KZ,好像我的输出不对。

请给些建议。

谢谢!