我用OPA2140(双运放SO8)做了一个比较器使用来放大一个小的方波信号,输出级对地并了一个10K电阻做假负载,然后有压敏电阻和自恢复保险丝做做过压过流,运放单供电DC12V,现在客户返回发现有一个运放输出的信号高电平只有两三百毫伏,结果静态量OUT脚与GND之间电阻只有10欧姆左右,请问导致这种损坏的原因有哪些?过压?短路?(芯片自有短路保护)还是其他?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
OPA2140内部也有 ESD保护电路了,
ESD Ratings
Human Body Model (HBM) 2000V
Charged Device Model (CDM) 500V