This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TRF37D73: 应用及注意事项咨询

Part Number: TRF37D73


我在TI官网上搜到了射频放大器,型号TRF37D73,增益:19.5dB,适用频率1-6000MHz。个人看频率及增益都符合我想增大CAT1发射功率的需求。

我们选用的CAT1模组主芯片是紫光展锐8910D,单天线(收发共用),模组最大输出功率23dBm,接收灵敏度-99dBm。我们产品应用环境恶劣,信号会被屏蔽,信号接收上可接受,但我们对于数据发送仍有较大需求,需要高速传输,提高产品发射功率,所以想在CAT1模组和天线之间加一颗TRF37D73。

问题:

1、不知TRF37D73是否适合我描述的应用?

2、使用上有什么注意事项?电源供电是否有要求?

3、初期想用TRF37D73EVM进行验证,有什么需要注意的?是否可以申请开发板样品?