各位前辈好!
我用OPA743搭建了一个反相器, 它工作正常, 也出了些问题.
OPA743数据手册里写到:
● WIDE SUPPLY RANGE: Single Supply: 3.5V to 12V Dual Supplies: ±1.75V to ±6V
但是,我在TINA-TI 仿真的时候, 只有采用双电源供电的时候, 才可以正常工作. 如果OPA743的V+接5V,V-接地(Vgnd)时, 输出电压没有反相,而且只有57mV 左右.
请教这是为何?
随帖附上仿真文件.
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
各位前辈好!
我用OPA743搭建了一个反相器, 它工作正常, 也出了些问题.
OPA743数据手册里写到:
● WIDE SUPPLY RANGE: Single Supply: 3.5V to 12V Dual Supplies: ±1.75V to ±6V
但是,我在TINA-TI 仿真的时候, 只有采用双电源供电的时候, 才可以正常工作. 如果OPA743的V+接5V,V-接地(Vgnd)时, 输出电压没有反相,而且只有57mV 左右.
请教这是为何?
随帖附上仿真文件.
谢谢!
这里的G=-1,而单电源供电的局限性就是输出不能低于GND,所以双电源供电可以解决这个问题。
单电源放大,可以将运放的输出端偏置在VCC/2的地方,然后输入正负电压的时候,输出以2.5V为基本参考。