This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH5401: 关于 LMH5401 输入、输出共模电压设置的问题

Part Number: LMH5401

LMH5401手册所标注的电气参数是在特定情况下测试的,即

at TA = 25°C, VS+ = 2.5 V, VS– = –2.5 V, VCM = 0 V, RL = 200-Ω differential, G = 12 dB (4 V/V), single-ended input,
differential output, and R
S = 50 Ω, (unless otherwise noted)

假设:输入信号的共模电压为0V,输出信号的共模电压为2V(VCM),供电电压为-0.5V和+4.5V,其他条件不变,那么器件的下面这些参数是否仍然符合手册描述呢?

GBP  SSBW  LSBW  SR  HD2  HD3