Part Number: AMC1301
问题1:如下图,这是一个说明图。A、B为供电端。例:前1秒钟,A=100V,B=GND。后1秒钟A=GND,B=100V。使用这个AMC1301测量检流电阻的正负电压。其中,器件的电源使用隔离电源,这个电源的地和AB系统的地不连接。电路能这样搭建吗?

问题2:我看这个器件的输入阻抗很低。怎么提高输入阻抗了,我能不能在AMC1301的正负输入引脚各接一个跟随器来提高输入阻抗。如果能接该具体怎么接了?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AMC1301
问题1:如下图,这是一个说明图。A、B为供电端。例:前1秒钟,A=100V,B=GND。后1秒钟A=GND,B=100V。使用这个AMC1301测量检流电阻的正负电压。其中,器件的电源使用隔离电源,这个电源的地和AB系统的地不连接。电路能这样搭建吗?

问题2:我看这个器件的输入阻抗很低。怎么提高输入阻抗了,我能不能在AMC1301的正负输入引脚各接一个跟随器来提高输入阻抗。如果能接该具体怎么接了?

刨除问题,如果一切能如你描述的那样实现,电路应该可以工作。
但有个疑问需要你衡量:“+120V_和GND_C一个系统”,"+5V_D、-5V_D和GND_D一个系统”,你是这样来规划的。
GND_C和GND_D通过10K电阻相连,猜想你希望以此将GND_D浮动,来满足高压下的运放工模输入电压范围问题。
显然,GND_D和GND_C无法隔离的。意味GND_D和GND_C最终将回流至同一个“GND”上。
这需要十分清楚电源架构的设计与实现。
祝你尝试成功。
为你推荐
感谢回答!是的。我将将GND_A和GND_D浮动,都是来满足高压下的运放工模输入电压范围正常。因为AMC1301的输入共模电压都是以它们的VCC_1系统的GND为参考的嘛。而AMC1301的输入电压不会超过几百毫伏,而VINN接的是自身的GND,那理论上输入的共模电压就是几百毫伏的一半了,就能满足共模电压要求了。另外关于电源的设计:其中A、B端点的120V使用的独立的T1外置电池,输出+120V_C和GND_C。系统供电由独立的另一块T2电池提供。T2电池通过三块隔离DCDC模块分别产生隔离电源(+5V_A、GND_A)。(+5V_B、GND_B)。(+5V_D、-5V_D、GND_D)。
另外为了确保待测电阻R3的电压小于250mV,我想对U3的输入VINP进行分压以确保输入小于250mV。使用分压电阻后为了减少对R3的影响我使用大电阻增大输入阻抗到10M欧。使用如下方法可行吗? 其中S1、S2、S3、S4 为模拟开关或者继电器开关提供选择连接。整个系统能这么设计吗?真的很急,真的麻烦你们了!