Part Number: THS6214
如上图中,当THS6214为±12V电源供电时,共模输入范围最小保证±9V,可以理解为下距电源轨3V吗?
当使用单12V供电时,是不是共模输入范围大约在3V-9V之间合适?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: THS6214
如上图中,当THS6214为±12V电源供电时,共模输入范围最小保证±9V,可以理解为下距电源轨3V吗?
当使用单12V供电时,是不是共模输入范围大约在3V-9V之间合适?
您好
1:可以理解为距电源轨3V
2:单电源情况下,共模范围通常与输入偏置、偏置电流和放大器的输入级设计有关,目前没有给出共模电压范围值。