This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

用FilterPro设计的滤波器理论值如何转化成工程实际电阻电容的值??

用FilterPro设计了一款滤波器,但电阻、电容值给的都是21.3n,75.4p等等,但在实际的电容没有这样的阻值,我该怎么做?滤波器电容的容值变化对截至频率影响很大,所以想问问技术大拿们,怎么处理这个实际应用问题的?

-------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------

电容和电阻一样有EIA认证的E12、E24等系列,但像X7R这种材料的电容,就可以引起15%/℃的变化,而E12、E24的容差误差值分别为10%,和5%,那电容的容差值该怎么确定呢?

  • 精密的电阻容易找, 但电容不易找, 你可以调整参数把精度换到电阻上.如果还是不能允许电容的偏差, 那常用的办法是筛选和校正, 使用可调电阻在生产中调试校正.

    你还可以跳开有精度问题的感容器件, 比如用滤波器或晶振来获得精确的频率的特性.

     

  • FilterPro工具在schmatic 界面可以调整电阻电容值为标准值的,记得是在右上角