Part Number: INA238
Other Parts Discussed in Thread: SYSCONFIG
1、涉及到的寄存器有SHUNT_CAL寄存器,写进去的值0x08CA,读到的值为0x084A;更换值,也会跟着变,但是不一致;
2、温度限制寄存器,写进去的值0x01FA,读到的值为0x00FA;更换值,也会跟着变,但是不一致。
3、芯片ID读取到的值与其他的寄存器的数据顺序是反的。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
“芯片ID读取到的值与其他的寄存器的数据顺序是反的。”
-------请参考数据手册“图 7-7”和 “图 7-8”,数据读写是高位在前。
请参考下面帖子,上拉电阻对I2C通讯的影响。
(+) INA237: 寄存器读取值与手册中不匹配 - 放大器论坛 - 放大器 - E2E 设计支持 (ti.com)
使用SysConfig工具可以帮助生成INA238的驱动代码: SysConfig (ti.com)
您好,谢谢回复
是这样,参照图7-7和图7-8读取的芯片ID的寄存器内容是正确的,但是我现在遇到的问题是,以这种方式获取的其他寄存器的值是反掉的,所以不知道问题在那里,ID的寄存器读取和其他寄存器的读取顺序是反掉的。比如: INA238_writeReg(sensor, INA238_adc_config_register, sensor->adcConfigRegister);写入的数值为0xFB68,根据高位在前,低位在后,回读的数据为0x68FB.芯片ID读取的为0x2381,相同的方式,读取到的寄存器却是反掉的,采用的是相同的读取函数。
取值不匹配的问题参考过以上文章,改过IIC上拉电阻,没有作用。当前采用的是4.7K,该总线上有其他IIC从站芯片,可以正常通信。
INA238的SHUNT_CAL寄存器和TEMPERATURE_LIMIT寄存器是主要错误的寄存器,回读的数据存在单字节错误。其他的配置寄存器没有任何问题。
母线电压/电流/温度的读取数据是错误的。而且存在不同的电压,读取的数据一直不变的问题。