Other Parts Discussed in Thread: TLV1701, , LM2903B
您好,我在用ADS软件导入贵公司电源电压在30V及以上的比较器时候,总是会报错,第一张图这是THS4601报的错误,没有定义limit函数,还有别的比较器TLV1701也会报错,报undefined model,如第二张图,不清楚是不是spice文件哪里出了问题,麻烦帮忙看一下,这两个报错属于是我在用ADS导入贵公司模型里经常出现的错误!希望可以得到解决!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
对于THS4601/tlv1701,建议使用PSPICE-FOR-TI工具来仿真。
您好,目前考虑到后续与其他电路的连接问题,所以还是用的ADS仿真,最近在ADS里我换了一种导入方式,是不会报错了,但是这个out输出好像和lib文件定义的管脚没有对上,这是我用lm2903b比较器搭的电路,.SUBCKT LM2903B IN+ IN- VCC GND OUT ,所以端口5是输出端,我命名为vo,但我在ADS里看输出端的信号时,选择pin name的时候有很多,就包含lib文件里的那些pin name,其中有一个是out引脚,然后这是我的输出结果,就是out引脚可以实现比较的功能,但是在lm2903b里没找到对应的管脚。麻烦老师们帮忙看一下!比较急!