Part Number: LMH6401
Can LMH6401 be used as a single-ended transfer differential? Can it be used to connect P to the signal and N to ground?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LMH6401
Can LMH6401 be used as a single-ended transfer differential? Can it be used to connect P to the signal and N to ground?
Yeah, the connection method is theoretically okay.
The P-terminal input signal of the LMH6401 during the test. The N-terminal is grounded. At this time, some P-terminal signals will be coupled in the N-terminal, resulting in the input signal of the LMH6401 becoming two signals in the same phase. The amplitude of the p-terminal is larger, and the signal coupled in the N is smaller, resulting in a smaller output signal amplitude of the LMH6401. Is it because of the connection method of the P and N inside the LMH6401?
Yeah