This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA228: I2C读操作_间隔时长要求

Part Number: INA228

INA228 85V、20 位、超精密功率/能量/充电监控器

关于以上这款TI芯片,在执行I2C读操作的时候,如果需要读两个bytes,主机这边会推两段clock,请问这两段clock之间的间隔时长有要求吗?如果间隔过长是不是会丢失后一个byte?

  • 您好,

          间隔没有要求。

         "SCL" 和“ACK By Controller" 都是I2C master(如MCU)提供的,

         需要注意的是如果工作在“continuous Mode"下,超过ADC的转换时间,数据会更新。