This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA281: 和ADS131b02 ADC搭配使用

Part Number: PGA281


现在用PGA281和ads131b02搭配使用,设计图如上图,当我在测量一个直流信号时,PGA281输入输出信号都是正常的,比如输入是0.074V,输出我用万用表测得也是0.074V,但此时ADS131b02读取出的数据却是0.063V,此时,我调整PGA281的增益,比如放大两倍,此时用万用表测得PGA281输出是正确的,放大两倍,但此时,ads131b02读取出的数据并不是正确的两倍(不是0.074×2,也不是0.063×2),会小于0.063×2。调整ads131b02也是类似的情况。

然后我将PGA281输出的端的R17,R19移除,将信号直接接入ads131b02,此时读取出的数据是准确的0.074V,调整ads131b02的增益,比如放大两倍,信号输出也是0.074×2,正确的。

对此我很迷惑,请前辈帮我分析系,是否我的设计是有问题的,感谢!