This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA228: INA228读取current值时出现加倍的现象

Part Number: INA228


测试电路如上图

待测电流源最大是10uA,当前测试输入8uA

Rshunt选择2Kohm,精度0.01%

则Vshunt电压范围是:

0uA*2000OHM~10uA*2000OHM    :0mV~20mV

CURRENT_LSB =8*Maximum Expected Current/ 2^19=10uA/2^19=0.0000191uA*8=0.0001528uA

ADCRANGE = 1时,SHUNT_CAL 的值必须乘以 4

SHUNT_CAL = 4*13107.2 x 10^6 x CURRENT_LSB x RSHUNT =7552(十进制)=0x1D80(16进制)

ADCRANGE = 0时,SHUNT_CAL 的值不用乘

SHUNT_CAL = 13107.2 x 10^6 x CURRENT_LSB x RSHUNT =1888(十进制)=0x760(16进制)

实测结果如下:current 的结果与实际输入8uA,都几乎变成2倍了,Vshunt的电压值都是准确的

ADCRANGE = 1

Vshunt

2F620

194080

15.1625mV

current

19B0F

105231

16.079uA

ADCRANGE = 0

Vshunt

0BD48

48456

15.1425mV

current

19A15

104981

16.0410968uA

补充下,如果断开电流源的输入,实测current也是很小的,只有30+nA,说明没有外部漏电存在。

请帮忙分析下,是哪里错误导致的,谢谢