你好,我有个技术问题,在选择运放时发现RC4580IDR的工作温度有点不清楚。请看截图。
在电气参数中都标注是-40~125度,可data sheet的第15页Package Information中确标注都是-40~85度,这个是什么意思?能解释一下吗?
还有,我用的是RC4580IDR,工作温度最高多少?如果功耗只有300mW,最高温度能到多少?
Package Information中的标注:
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,我有个技术问题,在选择运放时发现RC4580IDR的工作温度有点不清楚。请看截图。
在电气参数中都标注是-40~125度,可data sheet的第15页Package Information中确标注都是-40~85度,这个是什么意思?能解释一下吗?
还有,我用的是RC4580IDR,工作温度最高多少?如果功耗只有300mW,最高温度能到多少?
Package Information中的标注:
谢谢
datasheet看起来是矛盾了,但是根据TI产品的温度等级标准,RC4580I中的I代表的是Industrial,工业温度范围标准是-45~85度。
谢谢Kailyn
我想知道RC4580IDR能否用到125度??data sheet 中从头到尾的电气参数都是125度,为什么?
应该是数据手册写错了,–40°C to 125°C的是RC4580-Q1
谢谢Carter
请帮忙核实下,是否真是数据手册写错了,还是RC4580IDR能工作到85度?
这个对我很重要,谢谢。
好的,谢谢
期待你的回复。主要关心RC4580IDR能否工作到125度。
product engineer 昨天没有回复,由于有时差,请再等待一天,谢谢!
好的,期待专家解答。谢谢
顺便提下,如果运放功耗只有300mW能否在105度下工作?
如果芯片的温度范围只能到85度,那么即使300mW功耗也不允许超过85度工作。
不好意思回复的晚了,请参考:
Only the Q1 version has confirmed Ta = 125C operation.
The RC4580I will go back to 85C.
Hello Carter,
Thank you for your response. I am another customer to apply this part also with second source from ST. From the Datasheet we can see that, the maximum ratings table in page 4 of datasheet. From the table we can calculate the maximum power for this part is 1260mW. Can we think that the operating temperature for this part which can arrive at 85 centergrade with this power dissaption.
Normal understanding, the damage caused by temperature is the inside temperature instead of ambient temperature. So would you like to express to me what is the mechanism to evaluate the how much of the temperture the part can working?
Thank you in advance.