Other Parts Discussed in Thread: TIDA-01012, ADS8598S, INA146, ADS8885,
我认为,运算放大器在“正常”处理的输入电压的前提是“共地”。我认为,也就是:运算放大器输入的信号,正向输入端,反向输入端,两个目标被测量的信号的GND应该和TIDA-01012 的U5A和U5B 的GND是同一个GND,而后测量电路板才可以正常处理外部被测量的电压信号。现在问题是,TIDA-01012 的U5A和U5B GND明显不是输入的被测量电压信号的GND。
图纸疑问描述:此处的COM可以是被测量目标电路的GND,也可以是被测量目标电路上的某一个电阻的两端电压。如果“测量电路板TIDA-01012的COM连接器”是被接入了“被测量的目标电路板的GND”,我能理解为:仪表电路与目标被测量电路共地。相反,如果是电阻的两端电压,那么,这个电压恰巧还很大,例如:Vres =130V,那么,此处的COM在下面的Voltage Front End中,在进行被测量电压的分压处理,那么,然后,分压送入“运算放大器U5A,U5B”中,那么,我想问,这个U5A,U5B放大器是否可以正确处理输入进来的电压信号呢??毕竟仪表电路的GND和目标电路板GND不是一个GND啊。