最近正在做一个逆变电源的实验,其中采样电路是使用Ti的一款低输入偏置电流的运放TLV2314IDR作为差分放大电路去对来自逆变器直流母线电压、交流输出电压进行转换调理,然后再送入DSP28335的ADC采样脚中。但是在实际运行时,我将采样数据发送到上位机显示的波形会畸变,并且畸变程度还会随着我功率的增大而增大,使得我不得不再对采样数据进行一个低通滤波,而且发现如果只是辅电上电则不会出现这种抖动。下图依次为直流母线电压的差分电路(其他对交流电压的采样也是相同的电路)、辅助电源的电路、5V电源纹波的测试图以及上位机发送的经过软件滤波后的采样波形,其中辅助电源的5V电压纹波我实测大概是控制在10mV左右,所以我想应该也不会是运放供电电源的问题,怀疑是否是逆变器主电运行后带来的干扰到了采样差分电路中,不知该如何解决,求助各位大佬