This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMC1311-Q1: OUTP和OUTN的电压值相同,并不是差分输出

Part Number: AMC1311-Q1


大家好,应用原理图如下,R15修改为20KΩ,当HV_BUS输入电压为50V时,Vin=0.083V,与计算理论值相同((20KΩ/(12000kΩ+20kΩ))*50V=0.083V),此时OUTP=1.44V,OUTN=1.44V。我做了一个验证,把R7,R8,R9,R10,R11去掉,只保留R12,再次使用HV_BUS=50V测试,此时Vin=0.5V,OUTP=1.57V,OUTN=1.57V。
可以帮我看看是哪里的问题吗?为什么OUTP和OUTN的值是一样的?

Hello everyone, the application schematic diagram is as follows, R15 is modified to 20KΩ, when the input voltage of the HV_BUS is 50V, Vin=0.083V, which is the same as the calculated theoretical value ((20KΩ/(12000kΩ+20kΩ))*50V=0.083V), at this time, OUTP=1.44V, OUTN=1.44V. I did a verification, removed R7, R8, R9, R10, R11, only kept R12, and used HV_BUS=50V again, at this time Vin=0.5V, OUTP=1.57V, OUTN=1.57V.
Can you help me see what the problem is? Why are the values of OUTP and OUTN the same?