Part Number: LM358
如图是LM358规格书中的开环增益曲线(左)和闭环增益曲线(右),可见开环增益在频带内都是-20dB/dec,理论上来说,闭环增益的衰减段不是应该和开环增益曲线重合吗,但为什么G=-1和G=1时候的闭环增益高频部分明显和其他闭环增益曲线不重合,也和开环增益曲线不重合

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LM358
如图是LM358规格书中的开环增益曲线(左)和闭环增益曲线(右),可见开环增益在频带内都是-20dB/dec,理论上来说,闭环增益的衰减段不是应该和开环增益曲线重合吗,但为什么G=-1和G=1时候的闭环增益高频部分明显和其他闭环增益曲线不重合,也和开环增益曲线不重合

我认为你指的是运算放大器中的GBWP行为。GBWP是运算放大器增益响应的一阶近似值。当G=1时,LM358的Spice模型在单位增益响应处显示出增益峰值或Q效应,这意味着相位裕度将更低(根据数据表为56度)。如果设计或传递函数中存在Q,则单位增益带宽(UGBW)将受到影响,并推导出波特响应的实际交流响应。

通常,Q≤0.5 o(r阻尼系数≥1)意味着相位裕度约为90°。在这种情况下,G=1 AC响应曲线应遵循GBWP斜率,并与其余响应重叠(理论上)。
当G=-1时,情况略有不同。G=-1不符合交流响应中典型的重叠极点斜率行为,这是由于输出端感应出180°的反馈。波特图定义使用绝对增益图(负绝对值未定义),G=-1下的噪声增益实际上为2(RF/RI+1每G=-1运算放大器配置)。因此,如果将波特图向上移动到G=2,它应该与交流响应曲线其余部分的斜率重叠(理论上)。根据定义G=-1,由于定义-20log(增益),环路增益仍为0dB。