Part Number: PGA855
请问我PGA855的电路这样连接是否正确,我将LVSS连接到-15V,LVDD连接到+15V,后级的ADC是+-15V的
我实际电路通电时没有输出,断电才有输出,我想知道是芯片坏了还是电路接错
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
电路连接看起来正常。我没有看到U56的任何本地去耦/旁路电容器,它位于示意图的其他地方吗?
CFB(25pF)是否可能完全滤除放大器的输出?
Achieve High SNR with the PGA855, Fully Differential Programmable-Gain Amplifier
你能告诉我更多关于输入的信息吗(预期的电压和频率是多少)?选择了什么增益?
输入信号可能在设备的边界图之外: