Part Number: INA310A
The datasheet of INA310A3 states that the device has a PSRR of approximately 130 dB, but the latest PSPICE model simulation results show that the PSRR at low frequencies is only 77 dB, and the curve is also different from what is described in the datasheet. The same issue exists with the CMRR. Could this be an error in the PSPICE model?