This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV271电流采样失效问题

Other Parts Discussed in Thread: TLV271

如上原理图,为电机采样电流电路,额定电流为10A,调试过程中出现如下问题:

1、在待机情况下,即流过采样电阻R(0.003)上的电流为0A时,运放输入VP和VN处的电压波形相同,均为0.224V。同时,输出VO电压正常,为1.65V;

2、电机满载(10A)运行,开始阶段,运放VP、VN和VO电压均正常。2分钟过后,发现输出VO电压由1.65V慢慢降了下去,降至800mV,在VO下降过程中,

VP和VN波形一直正常。

尝试的解决办法:

测量所有电阻阻值,正常;去掉所有电容,更换运放TLV271,故障依然出现。

怀疑这个运放TLV271在手工焊接时容易失效,但是在采样电阻没有流过电流时,运放的输入、输出信号均正常。而当采样电阻流过大电流,10A时,输出掉了下去。能说明运放坏了吗?烦请定位一下故障原因,谢谢