Other Parts Discussed in Thread: TLC2272
如上图接法所示,一个同相放大电路,以2.5V做参考。
当我输入电压低于0.1V左右一下,使用较大放大倍数,输出可以达到4.99V,获得较接近电源电压的效果;
但是如果我输入电压为1V左右,较小放大倍数,在输入电压慢慢增大,输出就只有4.75V就达到了极限,请教这是什么原因?
使用是运放是TLC2272。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TLC2272
如上图接法所示,一个同相放大电路,以2.5V做参考。
当我输入电压低于0.1V左右一下,使用较大放大倍数,输出可以达到4.99V,获得较接近电源电压的效果;
但是如果我输入电压为1V左右,较小放大倍数,在输入电压慢慢增大,输出就只有4.75V就达到了极限,请教这是什么原因?
使用是运放是TLC2272。
我尝试使用了阻值较大的反馈电阻,可以较接近电源了。原先使用1k和1.6K实现2.6倍放大,输出最大电压Vmax=4.75;
现在使用10k和16K实现同样倍数的放大,输出最大电压Vmax=4.97;
这种问题是否可以理解为负载的原因?
有这方面的原因,毕竟反馈电阻也是负载的一部分。小信号大倍数放大时候如果反馈电阻选用小一点,是不是也不能达到接近电源电压?
可以运放的输出电流也都是几mA级别以上的,应该不至于这么容易受到反馈电阻不到1mA的影响吧