This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA228: ina228读取ID正确,可以正确配置,但是读取电流电压温度都是0

Part Number: INA228
Other Parts Discussed in Thread: INA237, INA238

目前做的两块板子都是此情况,测试时接入的电压为12V,芯片供电为3.3V
初始化代码
static INA228_State INA228_0_state = {

    /* Configuration and Settings */
    .configRegister = (INA228_config_register_rst_NormalOperation | \
                       INA228_config_register_rstacc_NormalOperation | \
                       0x0000U | \
                       INA228_config_register_tempcomp_Shunttemperaturecompensationdisabled | \
                       INA228_config_register_adcrange_16384mV),
    .adcConfigRegister = (INA228_adc_config_register_mode_Continuousbusvoltageshuntvoltageandtemperature | \
                          INA228_adc_config_register_vbusct_4120us | \
                          INA228_adc_config_register_vshct_4120us | \
                          INA228_adc_config_register_vtct_4120us | \
                          INA228_adc_config_register_avg_1024),
    .shuntCalRegister = 0x046BU,
    .shuntTempcoRegister = 0x0000U, /* TEMPCO is 0 ppm/°C */
    .diagAlrtRegister = (INA228_diag_alrt_register_alatch_Transparent | \
                         INA228_diag_alrt_register_cnvr_DisableconversionreadyflagonALERTpin | \
                         INA228_diag_alrt_register_slowalert_ALERTcomparisononnonaveragedADCvalue | \
                         INA228_diag_alrt_register_apol_Normalactivelowopendrain),
    .sovlRegister = 0x7FFFU,
    .suvlRegister = 0x8000U,
    .bovlRegister = 0x7FFFU,
    .buvlRegister = 0x0000U,
    .tempLimitRegister = 0x7FFFU,
    .pwrLimitRegister = 0xFFFFU,

    .adcrange = INA228_config_register_adcrange_16384mV,
    .currentlsb = 0.0001,

    /* Sensor's I2C bus ID and address */
    .busId = 0,
    .devAddr = 0x40U,

};
波形
读取代码
INA228_config(INA228_0);
  INA228_readReg(INA228_0,INA228_device_id_register);
  LCD_Init();//LCD初始化
  LCD_Fill(0,0,LCD_W,LCD_H,BLACK);
  /* add user code end 2 */

  while(1)
  {
     wk_usb_app_task();

    /* add user code begin 3 */
   
   
    vbus = INA228_getVBUS_V(INA228_0);
    // 显示电压值
    LCD_ShowFloatNum1(40,2,vbus,5,YELLOW,BLACK,24);
    current = INA228_getCURRENT_A(INA228_0);
    // 显示电流值
    LCD_ShowFloatNum1(40,28,current,5,0x07FF,BLACK,24);
    power = INA228_getPOWER_W(INA228_0);
    // 显示功率值
    LCD_ShowFloatNum1(40,56,power,5,WHITE,BLACK,24);
    temp = INA228_getDIETEMP_C(INA228_0);
    INA228_readReg(INA228_0,INA228_shunt_cal_register);