This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA 3116D2小声保护问题

TPA 3116D2无论设置为从模式还是主模式,当声音调到小时,FAULT脚一时为1一时为0,当声音调到最大时,正常,这是什么问题????

  • 亲;你的电路和原理呢?

  • 问题已经解决,将音频输入端1uF电容更换后OK,我用的是汤姆逊的105K100,不知道为什么这款电容不行,我换汤姆逊474也可以,目前使用普通的陶瓷电容

  • 太感谢你了。。。呵呵。。。

    我遇到的问题和你差不多。。。一共焊接4片板子,其中两片没问题,另外两片一上电就会DC detect,faultz一下为1,一下为0,也就是文档里说的420ms;

    最开始还以为是输出短路,,查了半天,没短啊,然后换芯片。。。还是一样。。没办法,,,还是看文档吧!faultz为0有3中情况,输出短路,过温和太高的DC offset,前两者都已经排除,就剩下DC offset了。。

    过高的DC offset 应该就会引起DC detect

    两种方法:1、上电时SD脚保持低电平,(我做了啊) 2、正负输入端阻抗匹配,我的P端运放跟随输出,N端接电容到地,按理说也算匹配吧(都是接4.7uF电容),,,没辙了。。。上论坛吧!
     
    结果就看到您的帖子了。。。天哪居然完美解决了我的问题,,
    因为我的4.7uF电容买过两次,,,不同一家店子买的,估计品牌不一样,,所以导致阻抗不匹配。。。然后重新把4.7uF都换了一遍,,天哪居然好了!!
     
     
    非常感谢!