最近设计了一块控制系统pcb,在使用过程中发现TL084I发烫特别严重,用温枪测了下,有55°,输入输出波形正常,±15V供电,请问TI工程师这种现象正常吗?有没有其他可以替代的产品,原先使用的一款OP07没有发现温度过高问题,工作温度就是常温。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TL084有四个通道,你用了几个通道?不用的通道怎么处理的?负载是什么
封装是啥?如果是8mA,+-15V,那么有240mW的功耗,热是正常的。如果觉得太热,可以使用两颗双运放,替换四运放。