This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA357: 希望寻找一个高带宽的运放料号,类似OPA357

Part Number: OPA357
Other Parts Discussed in Thread: OPA2673, LMH6720

你好,

现在有一个应用场景,有多个XO 并联,XO的输出幅度为0~3.3Vpp,频率100MHZ,希望能找到一个运放做为Buffer,能将XO的输出连接到负载设备上,最好这个运放能带EN Pin,希望给我推荐几个性价比比较高的型号。

  • 您好,

    根据您的要求提供的一些建议:100MHz 0-3.3Vpp 信号、缓冲器、EN 引脚或关断模式。

    1,OPA2673
    GBW = 600 MHz
    总电源= 5.75V 至13V
    2通道器件
    2,LMH6720
    GBW = 400 MHz
    总电源= 8V 至12V
    Vos = 6mV
    所有器件均具有单位增益稳定特性、并具有启用/禁用选项。 如果您有任何更具体的要求、请告诉我。

    以下链接提供了两款器件的详细比较:比较。