请推荐一款取代AD8129的运算放大器,因AD8129的DC PERFORMANCE中
Closed-Loop Gain Error 在±0.8 到±1.8%之间,请推荐一款这个参数优于0.1%的差分转单端运放,其他参数基本等同于AD8129,我的供电是±12V,输出1MHz时幅值能够达到±10.5V以上,输出驱动一段同轴电缆,需要低噪声,带宽在100MHz以上的差分转单端的精密运放。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
功能差不多的像THS4505,但此款供电最大不超过15V,看看THS4150这款吧。