This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA 可编程增益放大器选型



一般PGA放大倍数都是只有几个,例如 1 ,2 ,5,8。有没有放大倍数连续的的,并且带spi或者i2c接口的PGA芯片?

  • 你好!

    PGA放大器的放大倍数一般都是只有几个的,即使带SPI的,如PGA11X系列,因为其一般的地址位有3个或者2个,故一般放大倍数最多可选择的就8个。

    具体的PGA器件的查找:TI主页--放大器和线性器件—PGA/VGA,然后如果想使用SPI总线控制编程,可以选择可编程增益放大器,从中根据实际情况进行选择。

    谢谢!

  • 放大倍数连续可调的放大器主要有以下几种

    其中前五种是用模拟电压控制的,后面的VCA82X系统是用外部电阻来设计放大倍数的。

    目前这几种都不能用数字的SPI或I2C总线控制。

    推荐的方案是,用一个SPI或I2C接口的DAC 来设置增益控制电压的值。来实现连续可调。