This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

人体感应电压问题

Other Parts Discussed in Thread: LOG112

我使用的是贵公司log112对数放大器,从电路板上引出两根线到外部测量人体电阻。一根线是参考电源,一根线是log112的1(I1)脚;问题是人体只接触1脚,参考电源悬空,在没有回路的情况下测得电阻比较小,是什么原因?如何解决这个问题,谢谢!!!

  • 你好,在测试中使用人体作为Rref设置,最终反推出人体电阻的方式吗?

    这种方法有几点需要注意。

    1:共地点问题

    2:由于皮肤上电荷累计会出现共模电压问题。

    如果可能最好加入原理图和框架图。

  • 你好!

    对于LOG112的使用,除了要注意共地的问题之外,还要注意参考电流是有一定要求的,即I2<1mA,否则的话,其一致性会减小,即计算得到的结果存在一定误差,需要补偿,其次I1的电流最好满足I1<<1mA.

    其一致性曲线可参考DATASHEET的P7的VLOGOUT vs IREF。

    谢谢!

  • 补充一个问题:采用log112是用于测量人体电阻,电路调试好之后,量程内电阻测量基本正确,但是关机过了一段时间后,测量结果就有偏差。

    比如200K(电压2v)输入电阻调试好正确结果是-2.5V输出,关机过一段时间后再测量往上偏可能是2.7V,往下偏可能是2.35v.请问一下电路设计有什么缺陷吗?

  • 你好!

    从给出的数据来看的话,其电流应该不存在大于1mA的情况,其次,由于此电路中对于I1,I2会直接影响计算结果,出现上述的误差的主要来源可能是图中的圈出的两个电阻的误差造成的,滑动电阻的精度不高,而后面的是20G的电阻,精度应该也有限,再者请确认测试电阻的精度是否合适等。

    谢谢!