This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请问LM319输出的15V方波信号如何转换为3.3V方波信号?

各位老师好!

我现在通过LM319实现了一个过零比较电路,输出了一路20kHz、低电平0V~高电平15V的方波,我想要将此方波转换成为3.3V电平的方波,请问可以通过什么芯片或器件实现15V方波到3.3V方波的转换呢?

要求要响应速度比较快 ,100ns~200ns及以下比较适宜。

(LM319比较器在输出端上拉电压15V时,才能达到100ns响应速度。3.3V上拉时,响应速度会增加到500ns左右。所以希望增加一级方波电平转换芯片,但速度比较快才行。)

谢谢各位老师!!