请教,这个芯片能仅仅正电源工作吗?为什么?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好!
不是的。OPA124 供电电压范围为 ±5 ~ ±18, 或者单电源 10 ~ 36。
请问您的应用的供电电压范围是多少?
您好!我计划只用+12V可以吗?对于噪声以及稳漂方面有不利影响吗?
可以用+12V供电,对器件的本身的噪声和温漂不会有什么影响。单电源供电时,需要提供一个偏置电压,要保证这个偏置电压的稳定性。另外,OPA124不是R to R的运放,输入输出不会到达轨到轨,所以输入电压不能到0V。
请参照下面的文档,A Single-Supply Op-Amp Circuit Collection,全面的介绍了单电原供电运放电路。对你的问题会有很帮助。