This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMC3330: EMC辐射问题,次级地与系统(板卡)数字地相连后辐射超标

Part Number: AMC3330


原理图见上图,前级连接的线缆可以达到7m。

次级AGND与GND相连时,CISPR11标准辐射A级 31MHz左右的频点超标10多个dB;

断开AGND与GND的连接----去掉L2165,可以通过测试,而且裕量较多;

尝试过L2165更换为1兆欧的大电阻,也可以通过测试,但是功能会有问题。

请问有什么设计方面的建议或者有能PIN对PIN替代的器件也可以推荐

谢谢