Part Number: THS4532
Other Parts Discussed in Thread: LM7705, THS4531
我使用THS4532来驱动一款差分ADC,希望它能输出0V-2.048V,当输出0V时需要负电源,如果按照数据手册推荐的使用-0.23V作为负电源,无法输出真正的0V,经过测试似乎至少要-0.27V或-0.3V,为了对LDO电源选型,我在PSpice中进行仿真,却发现电流消耗超出我的预期。数据手册中的电流都是静态电流或者加上输出负载电流,
但是我使用50kHz信号作为输入,输出连接到压控电压源上获得单端信号,仿真消耗的电流需要11ma左右,这应该是正常的吧,不过和静态电流差距有点大,不过我好像没找到数据手册中关于工作电流的描述。但问题出在负电源上,下图是我的仿真原理图以及仿真结果。如果采用-0.23V作为负电源,不仅在输出0V时出现失真,而且负电源电流剧增,第二张图粉色曲线,达到-3A左右,这是怎么回事,如果采用-0.3V的话电流为0.4A左右,随着负电源电压绝对值的增大,消耗电流迅速降低,甚至当我采用-0.5时作为负电源,负电源的电流变成正数了,第三张图为采用-0.5V时负电源消耗的电流,按照电流路径本来正数应该是正常的吧,因为正电源的电流就是负的,那为什么前面的-0.23V时都是负电流。如果我的仿真有问题,还请指出,输出共模电压为1V,输入1V的正弦信号,放大后应该刚好在峰谷输出0V。