This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL072: 使用TL072CD 出现刚开机时噪音很大

Part Number: TL072


我司一款音频放大器产品,在使用了Date code: 2436, MADE IN:Malaysia 的TL072CD后发现刚开机时噪音很大,热机8-30秒后噪音会减小,每台产品需要用到三个TL072CD,只有在高音部分的电路中发现有噪音,低音不存在噪音。此音频放大器是成熟产品,量产将近十年,此前一直未出现过此类问题,帮忙看看是什么原因,谢谢!

以下是芯片信息:

MADE IN: Malaysia                 (1P)TL072CDR
2DC:          2Q:                      (Q) 2500    (D)2436+5  

LBL:18A (L)TO:1567                (2P)REV:A           (V)0033317

                                                 (20L)CSO:RFB   (21L)  CCO:USA

                                                 (22L)ASO:MLA   (23L) ACO:MYS