This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA814: 有源天线使用OPA作为低噪声放大器选型问题

Part Number: OPA814
Other Parts Discussed in Thread: OPA818, OPA817,

TI工程师:

      你们好,我们正在设计一款有源接收天线,工作频率是9KHz-30MHz,计划使用OPA作为低噪声的放大器,放大器增益要求20dB左右、并且具备很低的噪声。要求放大器的输入端具备极高的阻抗,以抵消天线输入端阻抗的失配。输出端匹配射频仪表的50Ω阻抗。还有注意到OPA放大器一般需要-5v的电压输入,-5v电压获得过程中,由于DC-DC转换带来频率谐波干扰,请帮忙推荐一款合适的放大器,最好是单正电源供电的。谢谢!

  • 对于上述增益所需的带宽,OPA818将是我们更好的选择之一,因为它是FET输入设备,并且在我们的其他选择中噪声最低。OPA817将是另一个不错的选择,因为OPA818的带宽可能会过大,但噪声性能不如OP818。我对-5V输入电压的含义有点困惑。我建议模拟电路,以确认电路将按预期运行。

  • 感谢推荐。-5V输入是指OPA814的VS-引脚输入的电压。电源设计时获得-5v电压需要DC转换,转换过程中产生频率谐波干扰,使得产品EMC指标失败。所以如果有单正电源供电的的OPA放大器,就不会产生这个问题。谢谢!

  • OPA814以及我们的大多数(如果不是全部的话)放大器都可以由单一电源配置供电,因此这不应该是一个问题。对于单电源配置中的任何放大器,都需要考虑设备的输入/输出范围。输入信号需要偏置到中间电源,而不是以地为中心。在设计单电源放大器时,这是一个常见的疏忽。