Other Parts Discussed in Thread: TMP112, LMT87
TI前辈您好:
我现在做的一个项目使用TMP112测量体温,需要提高测量精度,看了TMP112的数据手册,有两个疑问,恳请前辈不吝赐教!
(1)手册说要提高精度,在25度时校正下温度就可以了(电压因素先不管),0-50度的测量精度可以提高到0.175,不知道我的理解对不对?
(2)如果(1)说法对的话,是不是必须在25度温度下校正温度,其他室温行不行?
多谢!
如果用于测量体温的话,一般期望精度较高,我的理解是优于+/-0.1C吧。 TMP112的典型精度为0.5C@(0-65C),没有采取任何特别校准措施就可以保证的。应用中如果期望更高精度,可以采取校准的办法。数据手册中给出校准方法,大体上可以理解为分段折线校准的方式。你处应用是人体体温,可以将校准温度范围设置更窄一些,比如25C-45C。这个样可以采取多点折线校准或者基于最小二乘法的曲线拟合方法。确保测量精度需要注意的很多事情,以上描述只是器件软件应用的一些问题,在硬件设计中需要注意远离板上热源,不可以长时间通电防止自加热影响测量精度。
希望以上对你处应用有所帮助,此外除了TMP112其实还有LMT87等器件可以考虑。
Hi,
你的理解是对的,因为TMP112在室温25℃我们做了trim,保证误差在-0.5℃~+0.3℃,因此在做1点校准时要在25℃温度下。