Other Parts Discussed in Thread: AFE5801, AFE5807
前端放大器为差分输出,能驱动200欧姆或者号更大的差分 负载。The differential outputs of the MAX2034 are capable of driving a differential load impedance of 200Ω or greater. 这种情况该怎么样与后端100欧姆adc(AFE5801)相连?
谢谢了!
可以用变压器转,也可以选择可以驱动100欧姆的运算放大器。一般电流型的高频放大器可以驱动100欧姆的负载。
不明白为什么要MAX2034 LNA +AFE5801 ?
我们有全集成的AFE5807/8(8通道的LNA+VCA+ADC)和AFE58016/8(16通道的LNA+VCA+ADC),完全不需要分立的。