请问有谁遇到过这种问题没有?感觉Trctrl的3.3V会影响到CP的直流和低频噪声呢?Trctrl如果为低,频率也对,噪声也低。能通过其它的配置来消除这个影响不?
Hi, Jason
关于TrCtl,请参考手册中的如下功能解释:
The TrCtl pin not only controls the output port, but may also switch the output frequency simultaneously. For
example, if TrCtl = 1, the active port is RFoutTx with an output frequency of F1. When TrCtl changes from 1 to 0,
the active port could be RFoutRx with an output frequency of F2. LMX2571 has two sets of register to store the
configurations for F1 and F2.
当你切换逻辑电平时候,会把对应的频率设置在F1和F2两组寄存器配置之间切换,频率和相噪的差异可能是因为F1/F2的配置差异导致的。