AFE4404 IO_SUP/TX_SUP/RX_SUP 是否可以使用同一电压 3.0V ?
不可以,需要各自单独供电,请参考EVM板电路,http://www.ti.com.cn/cn/lit/ug/slau621a/slau621a.pdf
Demo板上 TX_SUP是5V的, 而RX_SUP and IO_SUP是由TPS7A4901产生的3V的。
RX_SUP和IO_SUP可以用同一个吗?AFE4404的datasheet上这样说:
IO_SUP: Separate supply for digital I/O. Must be less than or equal to RX_SUP. Can be tied to RX_SUP.
guangming wang1 说:IO_SUP
IO_SUP如果等于RX_SUP的话,可以用同一个。