这2个驱动芯片都带电流传感运放,如果不用这2个运放,管脚该如何处理? 不用运放可以正常工作吗?
另外麻烦推荐一个驱动DC电机的芯片,48v 15a 的指标。
谢谢
不用的运放不能直接悬空,就和多通道的运放,有未使用的道理一样,最简单的办法就是接成跟随器的形式。
这里的运放可以用来检测电流大小,数据手册中有给出它的作用,如果不适用的话,DRV8301也是可以工作的。
These can be used to sense a sum of the three half-bridges, two of the half-bridges individually, or in conjunction with an additional shunt amplifier to sense all three half-bridges individually.
48V的电机一般MOS管要选到两倍电压,驱动也是,TI现在还没有那么高电压的直流电机驱动芯片,可以用两个半桥驱动芯片搭一个,如果不要求电机正反转的话只需要一个半桥驱动芯片就够了,比如LM510x系列。http://www.ti.com/lsds/ti/power-management/half-bridge-driver-products.page
我现在想用drv8301 带mosfet 驱动48v 10a 的直流电机,电流采样用霍尔电流传感器采集相电流,不用drv8301自己的电流运放,不知道可行不