Other Parts Discussed in Thread: DRV8812, DRV8813, DRV8412
TI的工程师以及各位坛友:
我现在使用TI的电机驱动芯片时遇到一些问题,请各位高手指点。问题是这样子的,我使用DRV8812(驱动电流1.6A)驱动57步进电机,电机带载情况下在加速过程和高速(注:高速过程是匀速的,速度600RPM左右,这时候要是轨道摩擦力稍有不均匀就会失步)会有失步现象,如果把驱动芯片更换成DRV8813(驱动电流2A),在加速过程的失步可以解决,但是电机高速运转时,绕组线圈产生的反电动势也越大,由于绕组线圈电压与电流存在:du=L*di/dt的关系,在驱动芯片输入电压不改变的情况下,高速阶段的电流仍然没有办法提升,也就无法解决高速运转过程失步的问题,请问各位,这种问题怎么解决呢?