评估套件为新购,所有跳线均为默认状态,PC端使用的软件为PGA970EVMGUI。
1、PGA970EVM板不接外部电源的情况下,可以通过USB2ANY板与PC端建立通信,USB2ANY板上的指示灯上电时闪动,然后长亮,但是PC端所读到的寄存器数据全部为0,这种状态是否正常?
2、PGA970EVM板在外接DC12V(数据手册要求供10-30V电源)电源的情况下,所连接的USB2ANY板与PC端的连接会中断,PC端软件提示"HW DISCONNECTED",PC无法与PGA970建立通信,USB2ANY板上的指示灯闪亮,如何才能读取到PGA970芯片内部寄存器的数据?
3、PGA970EVM板在外接12V电源的情况下,测得TP6(AVDD)为2.85V(数据手册中为3V),TP9(DVDD)为1.86V(数据手册中为1.8V),这两个电压是否正常?
4、我的这套评估套件是否存在质量问题?