Other Parts Discussed in Thread: TDC7200
请问使用TDC7200测量方波的频率是否可以实现?大概的思路是利用MSP430自己发送一个START信号,然后STOP引脚接在待测信号源上,测量不同STOP信号之间的时间间隔,从而测量出频率。测试的时候外部的方波信号是满足TDC7200的电平要求的,使用模式2测量外部频率在100KHZ~1MHZ的方波时会出现测量出来的结果基本是没有规律的。但是如果使用MSP430自己模拟STOP信号的话测量非常稳定和准确。首先请问这种使用TDC7200的方法是否有问题,第二就是为何测量外部信号源的时候结果不稳定。(单片机模拟STOP信号和外部STOP信号的唯一区别是在单片机发出START信号时前者不会有STOP信号干扰,可能是这个问题?)