设计中使用外部时钟,图像传输正常,913的GPIO0配置为输出,914的GPIO0配置为输入,可以通过914的GPIO0控制913的GPIO0输出,但是913的GPIO1配置为输入,914的GPIO1配置为输出,无法从914的GPIO1读出913的GPIO1状态,如何配置才可以
913 寄存器0X0D配置 0x35,914 寄存器0x1d配置为0x13;
914 寄存器0x1d配置为0x13 没问题。
913 寄存器0X0D配置 0x35,这样的话bit6=0 0: Disable GPIO control from remote deserializer
0X0D的bit6=1 1: Enable GPIO control from remote deserializer
因此将0X0D配置的0X35 改为0X75 试试。