AWR1243发射信号调频周期、调频斜率和频点用户是否可控?求指点,急,谢谢...
你好,
是可控制的。
你可以参考这个雷达参数计算器,参数均可根据您的需求进行调整。
https://dev.ti.com/gallery/view/1792614/mmWaveSensingEstimator/
你好,
全部参数都可以通过API调整的。举个SDK提供的demo的配置参数例子:
profileCfg 0 77 353 7 133.33 0 0 30 1 256 2041 0 0 30
1.profile Identifier
2.start frequency in GHz
3.idle time in u-sec
4.ADC start time in u-sec
5.Ramp end time in u-sec
6.Tx output power back-off code for tx antennas
7.tx phase shifter for tx antennas
8.frequency slope constant
9.tx start time in u-sec
10.number of ADC samples
11.ADC sampling frequency in ksps
12.HPF1 (High Pass Filter 1) corner frequency 0: 175 KHz 1: 235 KHz 2: 350 KHz 3: 700 KHz
13.HPF2 (High Pass Filter 2) corner frequency 0: 350 KHz 1: 700 KHz 2: 1.4 MHz 3: 2.8 MHz
14.rx gain in dB (valid values 24 to 48)
你好,
同时发射时,chirp配置是相同的,分时发射时,chirp配置可以是不同的参数配置。
计算器只用于参数计算,配置信息设置使用这个工具:mmWave Demo Visualizer: SDK演示demo的GUI
https://dev.ti.com/gallery/view/1792614/mmWaveSensingEstimator/或https://dev.ti.com/gallery/
SDK指的是:mmWave SDK: mmWave Software Development Kit http://www.ti.com/tool/mmwave-sdk
建议可先看一下在线的视频培训:https://training.ti.com/mmwave-training-series
您好,我们现在对1243比较感兴趣,这里有几个参数希望在您这里确认一下。
1.发射信号的时宽、起始频率、调频斜率是否可以任意配置(在指定75~76G,77~81G范围内),还是只能在一定范围内?
2.我们看到每个发生器前段有一个移相器,那么三个发射器前端的移相器是分开配置还是统一配置?如何配置?
3.我们看到1243的俯仰角分辨率是14度,我们想知道单根天线的波束宽度是多少(方位向和俯仰方向)
最后有一个请求,希望您可以者告诉我这些资料是否在贵公司某个专门的网站上有。前段时间看您给的链接比较分散,我们希望更多了解1243这款产品,那些讲述整个系列产品的资料上的信息是否一定适用1242呢?
你好,
1.可任意配置。注意76-77只有1G带宽,77-81有4G带宽
2.分开配置。通过调用API进行配置。
3.俯仰角/水平角分辨率取决于您这边的天线排布方式,TI EVM的天线参数,请查看2.6节。http://www.ti.com/cn/lit/pdf/swru507
4.射频性能是一致的,区别在于处理器性能、基带放大器的带宽、ADC的采样率。
资料都能从产品页找到。http://www.ti.com.cn/product/cn/AWR1243/description
你好,
这几项参数是AWR1443/AWR1642才有的。这是内部带处理器的版本。
1243需要通过SPI口直接写寄存器。
你好,
请查看C:\ti\mmwave_dfp_00_09_01_06\docs\AWR1xx_Radar_Interface_Control.pdf
谢谢。
你好,
请查看该链接:https://e2e.ti.com/support/sensor/mmwave_sensors/f/1023/t/606772
您好,
感谢您对TI产品的支持与关注。
AWR1243只支持0 180度调制。
每一个chirp周期都能调整一次,取决于您的chirp的周期大小及chirp_idle时间(idle时间最小为几us),建议您使用在线计算器估算应用所需要使用的chirp参数。
链接为:https://dev.ti.com/gallery/view/1792614/mmWaveSensingEstimator/
谢谢。
那我为什么在interface document里看到:
Concatenated phase shift
for TX0/1/2,
b1:0 RESERVED (set it to
0b00)
b7:2 TX0 phase shift value
b9:8 RESERVED (set it to
0b00)
b15:10 TX1 phase shift
value
b17:16 RESERVED (set it to
0b00)
b23:18 TX2 phase shift
value
b31:24 Reserved
1 LSB = 360/2^6 = 5.6
degrees
5.6度是什么意思?
您好,
感谢您对TI产品的支持与关注。
针对后续产品的资料更新,请您持续关注TI官网的资料发布。
你好,
建议使用计算器进行计算https://dev.ti.com/gallery/view/1792614/mmWaveSensingEstimator/
如果是每个chirp的参数都相同,只需要考虑ADC/射频等重新开始采样的时间,约几个微秒。
如果是每个chirp的参数都不同,一次可以将最多4组,每组512个chirp参数写入到内部的ram里,执行时内部模块会直接调用,约几个微秒。
如果是每个chirp都进行实时的重新配置,需要考虑SPI传输数据需要耗费一定的时间。
你好,
一样的,你可以理解为射频系统的内部寄存器。
谢谢。
请联系代理或者到TI store购买
https://store.ti.com/
1243建议同时购买DEVPACK与TSW1400数据采集卡。
你好,
GUI界面源程序请查看GUI composer导入的源代码。
AWR1642 OOB demo传输的数据格式可查看以下位置的文档。
Hi,
The data saved in this file is the exact same data and format that is transmitted out of the mmWave device over the DATA_port. Users should see the mmWave demo doxygen in the mmWave SDK package to understand the format of the data and how to parse it.
Online Visualizer Link: 
To process the recorded data: See the Visualizer User's Guide, section 4.4, to understand what the data contains. Information on the actual data is available in the doxygen - <mmWave_SDK_Install_DIR>\packages\ti\demo\xwr16xx\mmw\docs\doxygen\html\index.html.
User's Guide:
There is a demo in beta that saves the recorded data to a human readable CSV file - you can read the code and understand the data conversion process:
mmWave visualizer with the LOG function: 
Thanks.