请教大神们,搭配TMP102 EVM的软件里,要怎么修改I2C地址位置?我有两块EVM,一个接地、一个我改接V+,但我找不到EVM的软件里哪里可以修改?或是有哪一套EVM的软件可以兼容?
我安装GUI看了下,是没有办法修改I2C slave 地址的,只能对配置寄存器以及T_LOW和T_HIGH进行配置。
I2C 7bit地址是通过ADD0的不同接法来实现更改的,在EVM user's guide中也有描述:
To configure one of four different addresses on the bus, connect the ADD0 pin to either the GND, V+, SDA, or SCL pin.