Other Parts Discussed in Thread: OPT101
opt101作为光探测器,检测反射光强,光源为650nm激光二极管。用基础应用的电路4,5脚接一起然后直接ADC采样,这样方案可行吗?是否需要输出之后再加放大电路?
看你光源输出的电流是多大了,如果是ua级别的话,用opt101直接放大接AD芯片就可以了。
OPT101实际是一款跨阻放大,内部集成了反馈电阻1Mohm,可以直接将4.5引脚接一起得到输出电压,但是需要看输出电压信号是否满足ADC输入范围,如果满足的话,可以直接给ADC。无需再放大。