从去年10月份开始使用PGA411-Q1替换ADI的AD2S1205,出货在6K/PCS,在不同客户那里遇到产品持续运行1-2周就会无故报警,目前大概有23台这样的情况。且是偶发性,同时在复位一次后,PGA411-Q1有能正常工作,出现问题的伺服电机功率主要集中在18.5KW-30KW的产品上(三相电机)。目前我们使用PGA411与MCU STM32F030没有使用SPI通讯,只使用了Fault和ABZ+光耦与MCU通讯。因此不能通过SPI知道具体什么原因引起的报警。初步怀疑为干扰引起的该问题,我当初替换AD2S1205设计时遇到SIN+和SIN-的滤波电容按照规格书上的68pF,就遇到SIN+的峰值过压报警(测试发现为很大的干扰),将68pF改为470pF后正常。不知道大侠们有没有好的建议?