适配于AWR1642的mmWave_Demo_Visualizer发送配置文件后,GUI没有任何结果显示

Other Parts Discussed in Thread: AWR1642, AWR1642BOOST

想用mmwave_sdk_01_02_00_05里的demo示例程序来验证AWR1642是否正常工作,但是通过GUI发送配置文件并点击“Record Start”之后,Plot里的结果显示界面没有任何反应,烧写程序或者debug模式下(CCS7.4)运行这两种方式都试过了,GUI都没有反应,请问有人遇到过类似的情况吗?

  • 老铁,我也是这个问题。
  • 你好,

    两个建议如下:

    1.建议检查一下串口配置,用于polt的串口是data port。如图左下角所示,连接成功会显示图中这种标识,请检查。

    2.如果确认连接成功,请检查console message中,sensorStart 有没有回复Done,如果没有,请检查配置文件及所烧写的SDK版本是否与GUI的一致。

    谢谢。

  • 你好,mmwave demo visualizer 中说SKD1.0   1.1   1.2的版本都兼容啊! 我的SDK是1.2.0.5,就是sensorStart 之后,没有返回Done。 

  • 您好!

    回答您的两个问题:

    1. 串口配置正确。

    2. GUI与SDK版本一致,但是sensorStart 没有回复Done。

    具体截图显示在下方了,请问您还有其它建议吗?




  • 你好,

    具体步骤你可以参考以下链接,进行比较。

    如何在xWR1xxx芯片上运行mmw demo

    E2E™ 设计支持
    Other Parts Discussed in Post: UNIFLASH , IWR1642 作者:TI 工程师 Chris Meng 本文基于的软件环境是mmwave_sdk_01_00_00_05和CCS7.1。本文测试使用的硬件是xWR1642 EVM,类似的方法适用于xWR1443 EVM。 用户需要预先安装好mmwave sdk,CCS和Uniflash。相关链接如下: mmWave SDK: mmWave Software Development...

    另外,附上成功运行的打印信息。SensorStart 后需要有Done,才能正常运行。

    谢谢

    mmwDemo:/>% ***************************************************************
    Skipped
    
    mmwDemo:/>% Created for SDK ver:01.02
    Skipped
    
    mmwDemo:/>% Created using Visualizer ver:1.2.0.0
    Skipped
    
    mmwDemo:/>% Frequency:77
    Skipped
    
    mmwDemo:/>% Platform:xWR16xx
    Skipped
    
    mmwDemo:/>% Scene Classifier:best_range_res
    Skipped
    
    mmwDemo:/>% Azimuth Resolution(deg):15
    Skipped
    
    mmwDemo:/>% Range Resolution(m):0.044
    Skipped
    
    mmwDemo:/>% Maximum unambiguous Range(m):9.02
    Skipped
    
    mmwDemo:/>% Maximum Radial Velocity(m/s):1
    Skipped
    
    mmwDemo:/>% Radial velocity resolution(m/s):0.13
    Skipped
    
    mmwDemo:/>% Frame Duration(msec):100
    Skipped
    
    mmwDemo:/>% Range Detection Threshold (dB):15
    Skipped
    
    mmwDemo:/>% Doppler Detection Threshold (dB):15
    Skipped
    
    mmwDemo:/>% Range Peak Grouping:enabled
    Skipped
    
    mmwDemo:/>% Doppler Peak Grouping:enabled
    Skipped
    
    mmwDemo:/>% Static clutter removal:disabled
    Skipped
    
    mmwDemo:/>% ***************************************************************
    Skipped
    
    mmwDemo:/>sensorStop
    Done
    
    mmwDemo:/>flushCfg
    Done
    
    mmwDemo:/>dfeDataOutputMode 1
    Done
    
    mmwDemo:/>channelCfg 15 3 0
    Done
    
    mmwDemo:/>adcCfg 2 1
    Done
    
    mmwDemo:/>adcbufCfg -1 0 0 1 0
    Done
    
    mmwDemo:/>profileCfg 0 77 429 7 57.14 0 0 70 1 256 5209 0 0 30
    Done
    
    mmwDemo:/>chirpCfg 0 0 0 0 0 0 0 1
    Done
    
    mmwDemo:/>chirpCfg 1 1 0 0 0 0 0 2
    Done
    
    mmwDemo:/>frameCfg 0 1 16 0 100 1 0
    Done
    
    mmwDemo:/>guiMonitor -1 1 1 0 0 0 1
    Done
    
    mmwDemo:/>cfarCfg -1 0 0 8 4 4 0 5120
    Done
    
    mmwDemo:/>cfarCfg -1 1 0 4 2 3 0 5120
    Done
    
    mmwDemo:/>peakGrouping -1 1 1 1 1 255
    Done
    
    mmwDemo:/>multiObjBeamForming -1 1 0.5
    Done
    
    mmwDemo:/>clutterRemoval -1 0
    Done
    
    mmwDemo:/>calibDcRangeSig -1 0 -5 8 256
    Done
    
    mmwDemo:/>extendedMaxVelocity -1 0
    Done
    
    mmwDemo:/>bpmCfg -1 0 0 1
    Done
    
    mmwDemo:/>lvdsStreamCfg -1 0 0 0
    Done
    
    mmwDemo:/>nearFieldCfg -1 0 0 0
    Done
    
    mmwDemo:/>compRangeBiasAndRxChanPhase 0.0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0
    Done
    
    mmwDemo:/>measureRangeBiasAndRxChanPhase 0 1.5 0.2
    Done
    
    mmwDemo:/>CQRxSatMonitor 0 3 5 123 0
    Done
    
    mmwDemo:/>CQSigImgMonitor 0 127 4
    Done
    
    mmwDemo:/>analogMonitor 1 1
    Done
    
    mmwDemo:/>sensorStart
    Debug: Init Calibration Status = 0x7fe
    
    Done

  • 另外,
    你可以尝试安装烧写1.1版本SDK进行尝试,更换一台电脑进行尝试。
    SDK链接:software-dl.ti.com/.../index_FDS.html
    谢谢
  • 您好,
    用两个1.2版本、1.1版本和1.0版本的SDK都试过了,Console Messages中的SensorStart均不返回Done。请问这应该是哪里的问题?
    另外,已经和TI员工联系过,这个问题的方案号是 AWR1642BOOST Issue SR#1-4446106565。
  • 另附上打印信息:

    mmwDemo:/>% ***************************************************************
    Skipped

    mmwDemo:/>% Created for SDK ver:01.02
    Skipped

    mmwDemo:/>% Created using Visualizer ver:1.2.0.0
    Skipped

    mmwDemo:/>% Frequency:77
    Skipped

    mmwDemo:/>% Platform:xWR16xx
    Skipped

    mmwDemo:/>% Scene Classifier:best_range_res
    Skipped

    mmwDemo:/>% Azimuth Resolution(deg):15
    Skipped

    mmwDemo:/>% Range Resolution(m):0.044
    Skipped

    mmwDemo:/>% Maximum unambiguous Range(m):9.02
    Skipped

    mmwDemo:/>% Maximum Radial Velocity(m/s):1
    Skipped

    mmwDemo:/>% Radial velocity resolution(m/s):0.13
    Skipped

    mmwDemo:/>% Frame Duration(msec):100
    Skipped

    mmwDemo:/>% Range Detection Threshold (dB):15
    Skipped

    mmwDemo:/>% Doppler Detection Threshold (dB):15
    Skipped

    mmwDemo:/>% Range Peak Grouping:enabled
    Skipped

    mmwDemo:/>% Doppler Peak Grouping:enabled
    Skipped

    mmwDemo:/>% Static clutter removal:disabled
    Skipped

    mmwDemo:/>% ***************************************************************
    Skipped

    mmwDemo:/>sensorStop
    Done

    mmwDemo:/>flushCfg
    Done

    mmwDemo:/>dfeDataOutputMode 1
    Done

    mmwDemo:/>channelCfg 15 3 0
    Done

    mmwDemo:/>adcCfg 2 1
    Done

    mmwDemo:/>adcbufCfg -1 0 0 1 0
    Done

    mmwDemo:/>profileCfg 0 77 429 7 57.14 0 0 70 1 256 5209 0 0 30
    Done

    mmwDemo:/>chirpCfg 0 0 0 0 0 0 0 1
    Done

    mmwDemo:/>chirpCfg 1 1 0 0 0 0 0 2
    Done

    mmwDemo:/>frameCfg 0 1 16 0 100 1 0
    Done

    mmwDemo:/>guiMonitor -1 1 1 0 0 0 1
    Done

    mmwDemo:/>cfarCfg -1 0 0 8 4 4 0 5120
    Done

    mmwDemo:/>cfarCfg -1 1 0 4 2 3 0 5120
    Done

    mmwDemo:/>peakGrouping -1 1 1 1 1 255
    Done

    mmwDemo:/>multiObjBeamForming -1 1 0.5
    Done

    mmwDemo:/>clutterRemoval -1 0
    Done

    mmwDemo:/>calibDcRangeSig -1 0 -5 8 256
    Done

    mmwDemo:/>extendedMaxVelocity -1 0
    Done

    mmwDemo:/>bpmCfg -1 0 0 1
    Done

    mmwDemo:/>lvdsStreamCfg -1 0 0 0
    Done

    mmwDemo:/>nearFieldCfg -1 0 0 0
    Done

    mmwDemo:/>compRangeBiasAndRxChanPhase 0.0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0
    Done

    mmwDemo:/>measureRangeBiasAndRxChanPhase 0 1.5 0.2
    Done

    mmwDemo:/>CQRxSatMonitor 0 3 5 123 0
    Done

    mmwDemo:/>CQSigImgMonitor 0 127 4
    Done

    mmwDemo:/>analogMonitor 1 1
    Done

    mmwDemo:/>sensorStart
  • 你好,

    请你更换一个电流大一点的电源适配器尝试。
    有相同情况发生,是因为电源适配器的原因。
    建议使用5V2A 或者5V3A电源适配器。
    谢谢。
  • 你好,请问1.2.0.5的安装包还有吗?能否给我发一份,万分感谢
  • 请问问题解决了吗?我遇到sensorStart 返回的是error -1